This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2634-Q1: Please help check the customer crystal parameter

Part Number: AM2634-Q1

Hi experts, 

Customer chooses a crystal with following parameter information: 

            Rated frequency is 25MHz; 

            Rated loading capacitance (shunt capacitance) is 8pF; 

            The frequency resolution under room temperature is +- 20 ppm and +-50ppm @ -40~125C

             ESR is 150Ω.

From the datasheet, we have the following parameters strictures: 

It seems like that the ESR and shunt capacitance are over the maximum limitation? I am not sure, so please help check it. 

Regards, 

Will