Part Number: TM4C129ENCPDT
Hi, when I'm trying to read the sensors on my board the following code works well to read the joystick values and the microphone. But it doesn't work for reading the accelerometers. Even though accelerometers are on x = PE0, y = PE1, z = PE2. And PE0 maps to CH3, PE1 = CH2 and PE2 = CH1.
See code below, thanks in advance.
#define JOYSTICKX 1
#define JOYSTICKY 2
#define MICROPHONE 3
#define ACCELX 4
#define ACCELY 5
#define ACCELZ 6
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOE)) {}
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_ADC0)) {}
GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_4); //Joystick Y
GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_3); //Joystick X
GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_0); //Accelerometer X
ADCSequenceConfigure(ADC0_BASE, JOYSTICKX, ADC_TRIGGER_PROCESSOR, 0);
ADCSequenceStepConfigure(ADC0_BASE, JOYSTICKX, 0, ADC_CTL_IE | ADC_CTL_END | ADC_CTL_CH9); //Joystick X
ADCSequenceEnable(ADC0_BASE, JOYSTICKX);
ADCSequenceConfigure(ADC0_BASE, JOYSTICKY, ADC_TRIGGER_PROCESSOR, 0);
ADCSequenceStepConfigure(ADC0_BASE, JOYSTICKY, 0, ADC_CTL_IE | ADC_CTL_END | ADC_CTL_CH0); //Joystick Y
ADCSequenceEnable(ADC0_BASE, JOYSTICKY);
ADCSequenceConfigure(ADC0_BASE, ACCELX, ADC_TRIGGER_PROCESSOR, 0);
ADCSequenceStepConfigure(ADC0_BASE, ACCELX, 0, ADC_CTL_IE | ADC_CTL_END | ADC_CTL_CH3); //AccelX
ADCSequenceEnable(ADC0_BASE, ACCELX);
ADCProcessorTrigger(ADC0_BASE, JOYSTICKX);
while(!ADCIntStatus(ADC0_BASE, JOYSTICKX, false)){}
ADCSequenceDataGet(ADC0_BASE, JOYSTICKX, &x);
ADCProcessorTrigger(ADC0_BASE, JOYSTICKY);
while(!ADCIntStatus(ADC0_BASE, JOYSTICKY, false)){}
ADCSequenceDataGet(ADC0_BASE, JOYSTICKY, &y);
ADCProcessorTrigger(ADC0_BASE, ACCELZ);
while(!ADCIntStatus(ADC0_BASE, ACCELZ, false)){}
ADCSequenceDataGet(ADC0_BASE, ACCELZ, &accZ);