Part Number: RM48L952
Hi,
As the previous thread got old and locked and the issues remains, I started a new thread.
Here is the old one: e2e.ti.com/.../rm48l952-crystal-circuit-recommendations

We did have an error in the calculation initially, but it had very small impact on the result.
Measuring the RMS current through the crystal gave us the following results for different series resistances:
0Ω showed 4.3mA and 740µW.
1.3kΩ showed 3.1mA and 384µW.
3.3kΩ showed 2mA and 160µW.
The series resistance is placed on OSCOUT from the MCU:

Looking at ECLK output, we can see the following for different series resistances:
- 0 Ohm: approx 45% duty cycle - 28 ns pulse
- 5k: approx 38% duty cycle - 24 ns pulse
- 18k: approx 9% duty cycle - 6 ns pulse
- 33k: doesn't start
- 75k: doesn't start
According to TI datasheet, 6ns is a limit for oscillator square wave input, but there are no limits for crystal operation.
Looking at ST devices datasheets, there are safety factor calculations for the crystal operation:



We are still looking for TI's recommendation on this topic. What is the limit for our device?
And, do you have any recommendations for specific crystals that are approved?
Best regards,
August Hultman