Part Number: AM2432
Other Parts Discussed in Thread: PROFIBUS, SYSCONFIG
hi Sir
1. Which GPIO of UART can support PROFIBUS function?
The PROFIBUS only work on UART0,don't it?
2.How do I set PRUSSn_UART_GFCLK Clock source to work on 12 MHz baud rate of UART ?
I want to test UART communation on frequence 12MHz?
PRU-ICSSG UART and PROFITBUS.
3.As below spec,Is the Error rate 12000000% when Baud rate on 12Mhz?

4.How to setup the configure to support 12-Mbps PROFIBUS?

BR
Sheng Yi