Part Number: LP-AM243
Hi,
In order to find if SPI works, I loaded the inbuilt example mcspi_performance_8bit_arm243x-lp_r5fss0-0_nortos_ti-arm-clang
and expected it to work. It did print a message saying "All tests have passed" but when I probe the SPI0 Data line, I do not see any activity on it. I do see clock being generated on the clock pin though but no activity on data lines and Chip select is also always in low state. I am probing the corresponding pins on Booster header. I later tried to use the api function MCSPI_Transfer but that fails right away with error code 3 (meaning transmission failed). What am I missing?
Thanks.