Hello
We have mcal driver for our project. We try to integrate also the freertos. So I have two important questions:
1. Could you enable us an example freertos project with mcal driver?
2. We want to initialize the first the peripheries of the controller and then start the Os. But this works with the syscfg settings; but not with the mcal drivers that we have. But when we start first the Os then no problem.
Which is the correct way and what must be done, that the Mcal drivers works like sysfg?
Thank you in advance