Part Number: TM4C1230E6PM
Hi,
I have several systems that communicate through the CANbus. Microcontrollers use ADC, master I2C, CANbus and systick. all ms, an ADC measurement request is made and every 100ms, I read data on the I2C. the microcontroller receive a request from the CANbus and reponse in a 1ms time base of the scheduler.
Only 1 system can reponse on a request, The ID for each systems is different.
I have 10 systems and in this Week, End, I have 4 who is resetted. (When I have a reset, I lost the power of the microcontroller). I don't have any timer of this problem but my customer who have this installation see a reset after many hour, but all systems isn't resetted.
Is it possible that the request can generate a fault in the microcontroller?
Best Regards,