I have a trouble about the LM Flash Programmer with version 1613 on Windows 11 platform.
The USB driver of JTAG is installed and shown in the windows device manager correctly.
When I click the program button of LM Flash Programmer to download the firmware, I get the error "unable to connect to target" from the LM Flash Programmer.
Then, I retry this step several times and can be successful one time.
Is there any bug or compatible issue in the LM Flash Programmer on Windows 11?