Part Number: MSP432E401Y
Hello, Good morning!
I just bought "LAUNCHPAD MSP432E401Y EVAL BRD". I ran the program used for MSP432P401R LaunchPad", but I got the error shown as below:
corlab4@corlab3(2034):./run.sh
Executing: "/home/corlab4/xb10/init/mcu/flash"/ccs_base/DebugServer/bin/DSLite flash -c user_files/configs/msp432p401r.ccxml -l user_files/settings/generated.ufsettings -s VerifyAfterProgramLoad="No verification" -e -f -v "user_files/images/uarti2c_MSP_EXP432P401R_XB10_nortos_gcc.out"
DSLite version 10.2.0.2249
Configuring Debugger (may take a few minutes on first launch)...
Initializing Register Database...
Initializing: CS_DAP_0
fatal: CS_DAP_0: Error initializing emulator: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the XDS110SupportReadMe.pdf file there for instructions. (Emulation package 9.3.0.00032)
Failed: CS_DAP_0: Error initializing emulator: (Error -260 @ 0x0)
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the XDS110SupportReadMe.pdf
file there for instructions.
(Emulation package 9.3.0.00032)
"./dslite.sh" command on line 15 failed with exit code 1.
corlab4@corlab3(2034):
I was told "MSP432E401Y EVAL BRD" should be compatible with "MSP432P401R EVAL BRD".