This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BeagleBone Black PRU-ICSS Soft UART won't enable additional UARTs

0

I want to activate more Serial Ports of the Beaglebone Black. Therfore I tried to activate the PRU-ICSS Soft UART. Firstly I made a new Kernel of the version: 4.19.94. There I configurated in menuconfig: PRU_REMOTEPROC to built-in. REMOTEPROC to built-in. TI_PRUSS to built-in. SERIAL_PRU_SUART to build-in. Then i cross-compiled the new Kernel in my old One without any errors.I added to the uEnv.txt:dtb=am335x-boneblack-prusuart.dtb

It booted up correctly with the boneblack-prusuart as device tree. However i cannot find the Serial Ports or something.

CPU  : AM335X-GP rev 2.1
I2C:   ready
DRAM:  512 MiB
No match for driver 'omap_hsmmc'
No match for driver 'omap_hsmmc'
Some drivers were not found
Reset Source: Global warm SW reset has occurred.
Reset Source: Power-on reset has occurred.
RTC 32KCLK Source: External.
MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1
Loading Environment from EXT4... ** File not found /boot/uboot.env **

** Unable to read "/boot/uboot.env" from mmc0:1 **
Board: BeagleBone Black
<ethaddr> not set. Validating first E-fuse MAC
BeagleBone Black:
BeagleBone: cape eeprom: i2c_probe: 0x54:
BeagleBone: cape eeprom: i2c_probe: 0x55:
BeagleBone: cape eeprom: i2c_probe: 0x56:
BeagleBone: cape eeprom: i2c_probe: 0x57:
Net:   eth0: MII MODE
cpsw, usb_ether
Press SPACE to abort autoboot in 0 seconds
board_name=[A335BNLT] ...
board_rev=[000C] ...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
gpio: pin 56 (gpio 56) value is 0
gpio: pin 55 (gpio 55) value is 0
gpio: pin 54 (gpio 54) value is 0
gpio: pin 53 (gpio 53) value is 1
switch to partitions #0, OK
mmc0 is current device
gpio: pin 54 (gpio 54) value is 1
Checking for: /uEnv.txt ...
1938 bytes read in 41 ms (45.9 KiB/s)
gpio: pin 55 (gpio 55) value is 1
Loaded environment from /uEnv.txt
Importing environment from mmc ...
Checking if uenvcmd is set ...
gpio: pin 56 (gpio 56) value is 1
Running uenvcmd ...
## Error: "loadall" not defined
debug: [console=tty0 console=ttyO0,115200n8 root=/dev/mmcblk0p1 rootfstype=ext4 rootwait] ...
debug: [bootz 0x82000000 0x88080000: 0x88000000] ...
Checking if client_ip is set ...
Checking for: /boot.scr ...
Checking for: /boot/boot.scr ...
Checking for: /boot/uEnv.txt ...
gpio: pin 55 (gpio 55) value is 1
2580 bytes read in 33 ms (76.2 KiB/s)
Loaded environment from /boot/uEnv.txt
debug: [dtb=am335x-boneblack-prusuart.dtb] ...
Using: dtb=am335x-boneblack-prusuart.dtb ...
Checking if uname_r is set in /boot/uEnv.txt...
gpio: pin 56 (gpio 56) value is 1
Running uname_boot ...
loading /boot/vmlinuz-4.19.94-ti-r42 ...
10088368 bytes read in 663 ms (14.5 MiB/s)
debug: [enable_uboot_overlays=] ...
loading /boot/dtbs/4.19.94-ti-r42/am335x-boneblack-prusuart.dtb ...
61245 bytes read in 93 ms (642.6 KiB/s)
uboot_overlays: add [enable_uboot_overlays=1] to /boot/uEnv.txt to enable...
loading /boot/initrd.img-4.19.94-ti-r42 ...
7050851 bytes read in 475 ms (14.2 MiB/s)
debug: [console=ttyO0,115200n8 root=/dev/mmcblk0p1 ro rootfstype=ext4 rootwait console=ttyO0,115200n8 root=/dev/mmcblk0p1 ro rootfstype=ext4 rootwait dtdebug=1] ...
debug: [bootz 0x82000000 0x88080000:6b9663 0x88000000] ...
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
   Using Device Tree in place at 88000000, end 88011f3c

Starting kernel ...

If i do

dmesg | grep tty

i only get shown ttyS0 that i am using to work with the beaglebone black. If i do

  dmesg | grep pru
dmesg | grep pru

or

    dmesg | grep serial
dmesg | grep serial

i get no output.

I also converted the dtb to a dts file and looked for "pru_suart". There is a pru_suart0 and a pru_suart1. I noticed that they both need a firmware.

firmware-name = "ti-pruss/pru_swuart-fw.elf";

However the file that probably needed is empty. And nowhere in the internet is something about this files .