Part Number: TMS570LS3137
Other Parts Discussed in Thread: TMDS570LS31HDK
Hello,
I write to have a confirmation on the spec of the signal EMIF_CLK:
The example at "17.2.5.6.1 Determining the Appropriate Value for the RR Field" and the whole "17.4 Example Configuration" chapters of the TRM set f(emif_clk) to 100MHz.
In the TMS570LS3137 datasheet, the "Table 6-27. EMIF Asynchronous Memory Timing Requirements" sets the minimum EMIF clock period to 11ns (i.e. up to 90.9MHz), but in the "Table 6-30. EMIF Synchronous Memory Switching Characteristics" the minimum EMIF_CLK cycle time is 20ns (i.e. a max frequency of 50MHz).
Can you please clarify which is the max EMIF_CLK to use for both SDRAM and async devices?
Thanks in advance,
Federico.