Part Number: TM4C129ENCZAD
Hello,
I want to have the option to disable the ethernet MAC and PHY of the TM4C129ENCZAD at the board level. I would like to know whether it is sufficient to leave the following dedicated pins unconnected:
- EN0TXOP/N
- EN0RXIP/N
- RBIAS
or whether additional circuitry is required.
Internally, from section 23.3.1.1 of the datasheet, I see that the SYCLK to the MAC can be gated off. I will plan to do that as well. I don't see a method for disabling the PHY.
I do also see that the power-down mode may be enabled as specified in 23.3.10. Please advise on how to properly disable ethernet.
Thank you.