Part Number: AM2634
Other Parts Discussed in Thread: SFRA
AM263x - is there an example project present to demonstrate Phase shifted Full Bridge control with AM2634 MCU.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Sorry, we dont have an example currently. It is currently not in the plan.
Are you trying to look for something like this from the Digital Power SDK:
We will try to support you through e2e with the syscfg configurations if you are trying to build an application.
May I know your complete requirement.
AM2634 Demos are placed in this link:
Regards
Sri Vidya
Hi SriVidya,
Yes, we are creating Peak Current Controlled Mode PSFB DC-DC Power Converter using AM2634.
currently in AM2634 demos there is no such example which demonstrates the PSFB.
i can see some demos available with TMS320 series MCUs.
Is it possible for you to share a demo project with AM2634 ?
Regards
Bikash
Hi Bikash
No currently we dont plan to create any example project for the Phase shifted Full Bridge. It is not planned for the release.
We will support you with the configuration. You can use the existing EPWM Trip Zone and CMPSS Trip examples in the SDK and carryout the implementation. If you are stuck or have any doubts regarding the configuration of EPWMS, we will support you through e2e.
i can see some demos available with TMS320 series MCUs.
Could you please share me link for this example or app note which is suitable for your requirement.
We can take a look and tell if it can be taken as reference for AM263. Because we made sure that the AM263 API routines have similar naming structure for easier porting from other device examples. If the APIs are same, you can very well try porting the same into AM263.
Regards
Sri Vidya
Hi Sri Vidya,
Thank You for reply.
I was referring to below example that is with C2000 Mcus,.
TIDM-02000-Peak Current Controlled Mode PSFB DC-DC Power Converter
I am trying to develop same with AM2634.
Regards
Bikash
Hi Bikash
I am looking at the C2000 project and see that the example has Control Driver APIs similar to AM263. So you can try porting it onto AM263.
On top level the following are the differences I see.
How do you test this software? Do you have the PSFB DC-DC of TI board with you? OR are you testing this with your custom board.
I am asking this because, the Control Card Pin Mappings Used in this project for C2000 might be different from the AM263. Its better to evaluate if all the module initializations are present in the AM263 before you start with the porting.
Let me know your inputs.
Thanks & regards
Sri Vidya
Thank You Srividya for your inputs.
For testing we are planning to use the PSFB DCDC board from TI.
Can we use this board together with AM263x eval board?
can you please help me with the product link?
BR
Bikash
Hi Bikash
What Product Link do you need?
or testing we are planning to use the PSFB DCDC board from TI.
You need to be careful with the pin mappings with AM263, especially the ADC pins. Which AM263 Rev board do you currently have?
Thanks & Regards
Sri Vidya
Hi Bikash
This board you are asking for is not owned by the AM263 team.
I am sharing with you the C2000 product links:
https://www.ti.com/tool/TIDM-02000
https://www.ti.com/tool/TIDM-PSFB-DCDC
Are you planning to purchase this board?
Regards
Sri Vidya