This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3359:How can I use the emac of cpsw and pru-icss at the same time?

Part Number: AM3359

I want to use EMAC of PRU-ICSS and EMAC of CPSW at the same time as a custom board using AM3359.
However, the IP setting is only for PHY of PRU_ICSS, and IP cannot be set for PHY of CPSW.
What should I do?

Oh, and
As I checked with debugging, it seems that the MAC address of CPSW is created.

In other words, I have uploaded the drivers of PRU and CPSW_EMAC, completed the basic setting, and even set the IP of PRU_EMAC.

As a result, setting the IP of CPSW will solve everything.

I use 'ndk_3_61_01_01', 'pdk_1_0_17'

thank you.