Part Number: AM2732-Q1
Other Parts Discussed in Thread: AM2732
Hi,
I tested with one TMDS273GPEVM connected to PC through USB cable, build below example and load the binary file on AM2732 board in ccs debug mode, run the program, open the memory browser, input L2 memory address such as 0x10280000, find read value is always 0xBAD0BAD0, try to write value but report error, while input L3 memory address such as 0x88000000 then can read the right value and also can modify it well.
So my question is can R5F L1/l2 memory be accessed through emulator when program is running? based on my test it is unable, i would like to know the reason, look forward to your reply, thanks.
mmwave_mcuplus_sdk_04_02_00_03\mcu_plus_sdk_am273x_08_02_00_26\examples\hello_world