Part Number: LAUNCHXL2-570LC43
Other Parts Discussed in Thread: DP83640
Are there any code examples of using the IEEE1588 capabilities on the ethernet phy either in the LAUNCHXL2-570LC43 or in the 570LC43 HDK ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LAUNCHXL2-570LC43
Other Parts Discussed in Thread: DP83640
Are there any code examples of using the IEEE1588 capabilities on the ethernet phy either in the LAUNCHXL2-570LC43 or in the 570LC43 HDK ?
The EMAC on TMS570LC43x doesn't support IEEE 1588. The Ethernet PHY DP83640 on TMS570 HDK supports IEEE1588 PTP.
Please find the PTP example supporting DP83640 PHY:
Hello QJ
Thanks for your input. However, it seems to contradict what it says in the web page for this launchpad:
https://www.ti.com/tool/LAUNCHXL2-570LC43?keyMatch=TMS570LC43X%20HERCULES%20DEVELOPMENT%20KIT
On the second paragraph it says this:
This LaunchPad features connectivity options such as IEEE 1588 precision time Ethernet PHY DP83630 and has the capability in addition to the standard BoosterPack headers, for further expansion to an FPGA or an external SRAM using high density connectors for MCU’s parallel interfaces - EMIF, RTP and DMM.
I have ordered an HDK from TI e-store, but while I wait for it to arrive, I should be able to run the example code you mention in the Launchpad that I already have, right?
Regards
Durga