Part Number: MCU-PLUS-SDK-AM263X
Hi expert,
This query is regarding the previous thread that I had raised - on how to debug an External Flash region.
(+) MCU-PLUS-SDK-AM263X: How to debug a Flash region? - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums
At the end of the conversation, I was able to finally enter into debugging mode. But then the address seem to be RAM rather than External flash when viewed through the disassembly.
Image-1: Debugging attempt for SBL QSPI example:
Image-2: Debugging attempt for GPIO LED blink example:
Is the intention of this below thread is to debug through QSPI into a RAM region, rather than debug through QSPI into an External Flash region?
(+) [FAQ] MCU-PLUS-SDK-AM243X: How to debug sbl_qspi (for am263 and am273) or sbl_ospi (for am243) or an application which is booted via OSPI/QSPI boot ? - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums
As stated in my initial thread, I am looking for an option to debug what has been flashed into the External flash region, rather than the RAM copy since it is of only 2MB size.
Kindly clarify.
Thanks & Regards,
Sharmili Narayanamurthy