Part Number: LM3S3748
Hi every body,
I have project with LM3S748 chipset, it very old MCU.
I make project with USB, before that i install pakage: "SW-EK-LM3S3748-5451.exe"
I check all USB examples in StellarisWare folder after install "SW-EK-LM3S3748-5451.exe" package.
I flash USB firmware but it seem don't work, check on device manager i don't see any new device on it.
I also debug in main of "USB_dev_bulk" example, the USBDBulkInit() return not nill.
So do any one meet same issue and have experience with LM3s USB family, please give me the suggestion?
thank you so much!
int main(void){
unsigned long ulTxCount;
unsigned long ulRxCount;
volatile tUSBDBulkDevice* myUSB;
char pcBuffer[16];
// Set the clocking to run from the PLL at 50MHz
SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
gpioInit();
g_bUSBConfigured = false;
SysCtlPeripheralEnable(USB_MUX_GPIO_PERIPH);
GPIOPinTypeGPIOOutput(USB_MUX_GPIO_BASE, USB_MUX_GPIO_PIN);
GPIOPinWrite(USB_MUX_GPIO_BASE, USB_MUX_GPIO_PIN, USB_MUX_SEL_DEVICE);
// Enable the system tick.
SysTickPeriodSet(SysCtlClockGet() / SYSTICKS_PER_SECOND);
SysTickIntEnable();
SysTickEnable();
// Initialize the transmit and receive buffers.
USBBufferInit((tUSBBuffer *)&g_sTxBuffer);
USBBufferInit((tUSBBuffer *)&g_sRxBuffer);
myUSB = USBDBulkInit(0, (tUSBDBulkDevice *)&g_sBulkDevice);
if(myUSB->usVID == 0x1cbe){
GPIOPinWrite(GPIO_PORTG_BASE, GPIO_PIN_0, GPIO_PIN_0);//ADD MORE: GPIO_PIN_0 is high so USBDBulkInit() return USB VID: 0x1cbe
}else{
GPIOPinWrite(GPIO_PORTG_BASE, GPIO_PIN_0, 0x00);//ADD MORE
}
if(myUSB->usPID == 0x0003){
GPIOPinWrite(GPIO_PORTG_BASE, GPIO_PIN_1, GPIO_PIN_1);//ADD MORE: GPIO_PIN_1 is high so USBDBulkInit() return USB PID: 0x0003
}else{
GPIOPinWrite(GPIO_PORTG_BASE, GPIO_PIN_1, 0x00);//ADD MORE
}
// Clear our local byte counters.
ulRxCount = 0;
ulTxCount = 0;
// Main application loop.
while(1){
// Have we been asked to update the status display?
if(g_ulFlags & COMMAND_STATUS_UPDATE){
// Clear the command flag
g_ulFlags &= ~COMMAND_STATUS_UPDATE;
}
// Has there been any transmit traffic since we last checked?
if(ulTxCount != g_ulTxCount){
// Take a snapshot of the latest transmit count.
ulTxCount = g_ulTxCount;
}
// Has there been any receive traffic since we last checked?
if(ulRxCount != g_ulRxCount){
// Take a snapshot of the latest receive count.
ulRxCount = g_ulRxCount;
}
}
}