This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCU-PLUS-SDK-AM243X: Periodic task in bootloader

Part Number: MCU-PLUS-SDK-AM243X

Hello Expert,

I have two questions regarding bootloader.


Can bootloader run multiple tasks? What I am aiming for is periodic GPIO led blink during booting. Is this possible?

Could you describe how to debug the bootloader. I know I need to use loop_forever(); However I am not sure on how to connect debugger.
When I load to flash the  ospi bootloader and try to connect via code composer studio I can see that the processor is executing the same 
addresses repeatedly. Hinting that it is running in the loop. But I cannot load see which code line it is on, variables and so on..
Is the process of connecting different?

Thank you for your answer

Dominik Ondra