This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0L1306: An external wake source for STANDBY

Part Number: MSPM0L1306

Hi,

My customer wants to use multiple external wake sources in MSPM0L1306.
The operating mode is STANDY0/1 mode.

I understood any GPIO pins can be wake up the system from STANDY with asynchronous fast clock request.
But the wake up source can be detected after wake up?
For example, there are three external events, DIO0, DIO1 and DIO2.
After the wakeup, the software understand which GPIO triggered the wakeup?
GPIO MIS(Masked Interrupt Status) registers work?

Thanks and regards,
Koichiro Tashiro