Part Number: MSPM0L1305
Other Parts Discussed in Thread: MSPM0L1306, , LP-MSPM0L1306, MSPM0G3507
Dear TIer
I use MSPMOG3507 Time's input capture,obtaining time after GPIO status,but don‘t read GPIO status。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSPM0L1305
Other Parts Discussed in Thread: MSPM0L1306, , LP-MSPM0L1306, MSPM0G3507
Dear TIer
I use MSPMOG3507 Time's input capture,obtaining time after GPIO status,but don‘t read GPIO status。
Hi Jinlong,
Can you elaborate on the issue you are seeing? If you want to read a GPIO, you can use the Driverlib DL_GPIO_readPins() API.

Also, you should be using the examples under the <install location>\mspm0_sdk_0_54_00_03_eng\examples\nortos\LP_MSPM0L1306 directory of the SDK with this device.
Best Regards,
Brandon Fisher
Thank you for your reply.
GPIO state can be read correctly, but not after input capture。
Hi Jinlong,
Have you modified the code at all?
I would also point out that the default pin for the switch used in the example you mentioned is not compatible with the MSPM0L1305. Hence why you want to use the example in the LP-MSPM0L1306 directory.
Regards,
Brandon Fisher
MSPM0G3507 not include Part number options。Are they very different in GPIO and time?
Hi Jinlong,
You can reach out to your TI representative for more information on MSPM0G3507. It will have different available GPIOs than MSPM0L1306/1305 though.
Best Regards,
Brandon Fisher