This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-AM243: FSI external trigger for ping transmission

Part Number: LP-AM243

Hi experts,

I am working on the LP-AM243 (E2) having questions about external triggering of ping transmission of the FSI unit:

- Where can I find a list of the external trigger sources of the EXT_TRIG_SEL field in the FSITX0_TX_PING_CTRL_ALT1_Register (14h)?

- Which configurations are required to activate period ping transmission, e.g. via an ePWM? As far as I understand it is necessary to: 1) enable external trigger sources via the EXT_TRIG_EN in the FSITX0_TX_PING_CTRL_ALT1_Register (14h), 2) select the corresponding source via the EXT_TRIG_SEL field in the FSITX0_TX_PING_CTRL_ALT1_Register (14h) and 3) activate external triggering in the START_MODE field in the FSITX0_TX_OPER_LO_ALT1_Register (8h).

Thanks for your help!

Regards,

Jan