This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2634: External flash option S25FL064L can I use the SBL flashing program of the SDK?

Part Number: AM2634
Other Parts Discussed in Thread: SYSCONFIG

Hi Team,

There's an issue from the customer need your help:

When debugging with the AM263 CC board, I went into QSPI boot mode using the SBL of the SDK to successfully flash the program. However, the external flash used by the CC board is S25FL128S, and the flash configuration in sysconfig is only S25FL128S. If I use S25FL064L external flash, do I need to reconfigure and flash? Can these two chip programming methods be used in common?

Could you help check this case? Thanks.

Best Regards,

Ben