Other Parts Discussed in Thread: TDA4VM
Hi Team:
The CPU I/O usage is too high when I write to eMMC, we found that the CPU io usage range was between 20% and 80%. Is this performance normal?
How can I solve the problem?
The chip is TDA4VM and software version SDK7.3

top:
Mem: 2286656K used, 169984K free, 502656K shrd, 45632K buff, 1519616K cached
1.CPU: 8% usr 11% sys 0% nic 0% idle 77% io 2% irq 0% sirq
2.CPU: 6% usr 16% sys 0% nic 22% idle 51% io 2% irq 0% sirq
3.CPU: 8% usr 18% sys 0% nic 35% idle 33% io 2% irq 0% sirq
4. CPU: 8% usr 22% sys 0% nic 42% idle 23% io 2% irq 0% sirq