Part Number: AM2634-Q1
Hi BU,
In my customer's board, the following power up sequence is found. 
The green signal is PORz, blue signal is WARMRSTz, yellow signal is 1.2V VDD, and the pink signal is the crystal oscillator.
From the waveform, it seems that the t_WARMRSTz not meet the AM263x power-on sequencing requirement in Datasheet:

Please help check if this is fine or not.
From my understanding, the WARMRSTz pin is de-asserted by device but not peripheral circuit during power-up phase. So it will be ok?
BR,
Will