Part Number: TM4C129XNCZAD
Dear Sir,
I am try to use boot loader on UART1 for controller TM4C129XCNZAD
I want to use UART1 for update of code.
The PORT Use as PORTQ and pin 4 and Pin 5
// PQ4-5 are used for UART1.
ROM_GPIOPinConfigure(GPIO_PQ4_U1RX);
ROM_GPIOPinConfigure(GPIO_PQ5_U1TX);
ROM_GPIOPinTypeUART(GPIO_PORTQ_BASE, GPIO_PIN_4 | GPIO_PIN_5);
Initialization of UART1 as describe in Sample example.
void Uart1_PC_init(uint32_t ui32SysClock)
{
MAP_GPIOPinTypeUART(GPIO_PORTQ_BASE, GPIO_PIN_4 | GPIO_PIN_5);
MAP_UARTConfigSetExpClk(UART1_BASE, ui32SysClock, 9600,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE));
MAP_IntEnable(INT_UART1);
MAP_UARTIntEnable(UART1_BASE, UART_INT_RX | UART_INT_RT);
}
The blconfig.h was modified for above UART1 but not working.
I have some doubt that the setting done by myself have issue .
Can you check for UART1 for above configuration. Attached blconfig.h
Regards,
Rajesh Varma