Part Number: MSP-EXP432E401Y
Other Parts Discussed in Thread: DAC8568, , BOOST-DAC8568
Hey I have the MSP-EXP432E401Y and the DAC8568. I noticed that the pinouts between these devices are most likely not compatible. The spi clk pin on the board in one pin higher than the sck pin on the DAC. The MOSI pin is also one pin higher than on the board. This cannot be fixed by moving the board up 1 pin because then the 5V and ground pins will not be aligned properly. Is there a boost DAC that is compatible with launchpad?