Part Number: TM4C123GH6PM
Other Parts Discussed in Thread: UNIFLASH
Hi Folks,
Has anyone had success using the XDS110 Debug probe and programming the flash of a TM4123GH6PM (TIVA) chip?
Some background info. I've been using a LM Flash Programmer and a devkit (Stellaris Development Board) to program my custom board.
Using LM Flash I can download all 256K of the TIVA chip and flash other chips using the LM Flash Programmer setup.
My challenge comes when I want to simplify the setup and just use a XDS 110 Debug Probe. I can successfully erase the chip using Uniflash, but I can't seem to write the image. It gives me the following errors:
[17:57:54] Begin Launching session operation.
[17:57:54] CORTEX_M4_0: GEL Output:
Memory Map Initialization Complete
[17:57:55] Operation Launching session returned.
[17:57:55] Loaded target configuration from: C:\Users\rshan\AppData\Local\TEXASI~1\CCS\TI\0\0\/temptargetconfiguration.ccxml
[17:57:55] Settings purged.
[17:58:36] Start operations on multiple programs on the target core...
[17:58:37] Loading program: D:\ti\tiva\TIVA_PK_M1_DEC24\TIVA_FLASH_LOADS\boot_plus50K_plus150K_ver1201.bin
[17:58:37] ERROR >> CORTEX_M4_0: GEL: Encountered a problem loading file: D:\ti\tiva\TIVA_PK_M1_DEC24\TIVA_FLASH_LOADS\boot_plus50K_plus150K_ver1201.bin Could not determine target type of file
[17:58:37] Encountered a problem loading file: D:\ti\tiva\TIVA_PK_M1_DEC24\TIVA_FLASH_LOADS\boot_plus50K_plus150K_ver1201.bin
Could not determine target type of file
[17:58:37] Programs operation finished.
Thanks much for any suggestions. Maybe I need to convert the .bin file to some other format?
Bob