This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: Selection of DATA and ADDRESS lines

Part Number: AM2434

Dear sir,

Which all lines can i used as data and address lines other than DDR4 interface to interface the devices like External ADC,CPLD,MRAM etc.?

Regards,

SANDHYA

  • Hello Sandhya,

    There are multiple communication peripherals in the AM243x SoC that may be used to interface with external devices other than DDR4. I would recommend looking into GPMC and ICSSG peripherals as possible options for more complicated interfaces then the standard SPI, I2C, or UART.

    The AM243x ALV package DDR pins are dedicated to the DDR4/LPDDR4 interface only and cannot be used for alternative functions.

    Best Regards,

    Zackary Fleenor