Part Number: TMS570LC4357
When debugging with the Trace32 Lauterbach probe and recording traces via the ETM module, it was observed that depending on the selected ETM port size, the processor execution time varied. For example, execution was about 3 time faster when using a 32 bits port vs an 8 bits port.
Can you confirm that the ETM induces "wait" state in the processor if it does not have the bandwidth to output all required trace data on the ETM port otherwise (for example, because it is smaller)?