Part Number: TM4C129XNCZAD
Dear Sir,
I am try to use boot loader on UART1 for controller TM4C129XCNZAD
I want to use UART1 for update of code.
Steps:
1. I had dumped the bconfig.h code supplied with demo board @0x0000 with Jlink
The application address is 0x4000
2. I had dumped the another code through Jlink @0x4000
3. I had dumped the another code through UART1 and LM Flash Programmer at baud rate with configured in bconfig.h @4000 adress
Its working.
My question is that While dumping code through UART if power interrupt or gone then Programme through UART is stop working.
How to handle that
Regards,
Rajesh Varma
Regards,
Rajesh Varma