Part Number: AM2434
Other Parts Discussed in Thread: UNIFLASH
Customer having same issue with both LP EVM and custom board
The result seems to be different depending on the erase-size specified.
When erase-size over 0x200000 (2Mbyte) is specified in hexadecimal, an error will occur. but If erase-size less than this is specified, it succeeds.
(this result is on the AM2434-LP)
Are there any specifications or restrictions on size specifications?
Command Line Log:
setok@workstation ~/ti/mcu_plus_sdk_am243x_08_02_00_31
% python3 tools/boot/uart_uniflash.py --flash-writer=./tools/boot/sbl_prebuilt/am243x-lp/sbl_uart_uniflash.release.tiimage -p /dev/ttyACM0 --operation=erase --flash-offset=0 --erase-size=0x300000
Found flash writer ... sending ./tools/boot/sbl_prebuilt/am243x-lp/sbl_uart_uniflash.release.tiimage
Sent flashwriter ./tools/boot/sbl_prebuilt/am243x-lp/sbl_uart_uniflash.release.tiimage of size 315416 bytes in 28.5s.
Sending erase command: 1031bytes [00:11, 9302.17bytes/s]recv error: getc timeout in start sequence
Sending erase command: 1032bytes [00:11, 62.39bytes/s]^C
[ERROR] XMODEM recv failed, no response OR incorrect response from EVM OR cancelled by user,
Power cycle EVM and run this script again !!!
setok@workstation ~/ti/mcu_plus_sdk_am243x_08_02_00_31
% python3 tools/boot/uart_uniflash.py --flash-writer=./tools/boot/sbl_prebuilt/am243x-lp/sbl_uart_uniflash.release.tiimage -p /dev/ttyACM0 --operation=erase --flash-offset=0 --erase-size=0x200000
Found flash writer ... sending ./tools/boot/sbl_prebuilt/am243x-lp/sbl_uart_uniflash.release.tiimage
Sent flashwriter ./tools/boot/sbl_prebuilt/am243x-lp/sbl_uart_uniflash.release.tiimage of size 315416 bytes in 30.23s.
Sent flash erase command.
[STATUS] SUCCESS !!!