Part Number: AM2432
At present, I have made an AM2432 board, but can not download the program; Could you tell me how to solve the problem? Are there detailed procedures for programming into RAM and external flash?CCS for the development environment
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM2432
At present, I have made an AM2432 board, but can not download the program; Could you tell me how to solve the problem? Are there detailed procedures for programming into RAM and external flash?CCS for the development environment
Hi,
Please specify what AM2432 board you have made and the MCU+ SDK version you are using.
I assume it is a customer board using AM2432. The answer is depending on the customer board
If you have a JTAG emulator (XDS-110) on board, then you can load your application code using JTAG.
If you do not have JTAG built-in on board, then you can only use the UART or SD card to bootload your application code.
Best regards,
Ming
Hi,
Are you booting over UART, or QSPI, or MMC? Is this a board of your own design, or is this one of the TI EVM designs. Are you able to get any output from the SBL over UART? Can you share that if so?
Thank you,
-Randy
Hi,
Please let me know if you need assistance on this topic any further.
Thank you,
-Randy