This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EK-TM4C1294XL: One Second timer Interrupt

Part Number: EK-TM4C1294XL


Hi,

I want a timer which generates every one second. I have tried the code attached in that i changed load value . but didnot worked, Also i notice that system clock is set at 120MHz but when geting it using SysCtlClockget(), it return 9.6MHz  why? I calculated and tried both 120MHz & 9.6MHz based Timer load value but not getting exact one second interrupt.

Please Help

Regards

Khodidas 


/*
 * Author : - KHODIDAS DOMADIYA\
 * Organization: - Optimzed Solutions Ltd.
 * Department: -Product ENgineering services.
 *
 * Date:- 12-05-2021
 *

 *LED4 PH3  //INDICATION LED
 *LED5 PF1  //ETHERNET LED
 *LED6 PF4  //ETHERNET LED
 *If PSFLT =1 Then powersupply OK,
 *Indicate TO MAIN as PSFLT
 *
 * If FROM MAIN =1 then Start Monitoring,
 * If LOCKING/TRIPPING =1 then Condition/Health OK
 * IF ARC,IDSLW,TEMP,MAIN_IN =1 Then Signals are OK
 *
 *
 **UPDATED ON 22-06-2021
 * =>AS per Discussion, After poweron and start command,PSFLT must be monitored, it indicates the powersupply fault signal, ifit is low then powersupply is faulty
 * so do not start monitoring, control and data transfer and generate LOCKING/ TRIPPING as well as TO MAIN (indication to Mainboard,)
 *
 *=>according to discussion that On REEAD command, read and send data to ethernet ,erase and reset entire device.ERASE or RESET command is not to be given.
 *=> Add DIAGNOSTIC Mode, in that during runtime, thresholds can be changeable. and in RUN/NORMAL Mode it is to be set before START command
 *=>
 *=> IP ADDRESS USED IS STATIC
 *
 *        RF_FORWARD_VAL= ADC_OUT_1[2];           //PE3
 *        RF_REVERSE_VAL= ADC_OUT_1[3];           //PE2
 *        TEMPERATURE_VAL=ADC_OUT_1[4];           //PK0
 *        VDS_VAL        =ADC_OUT_1[5];           //PK1
 *        ID_VAL         =ADC_OUT_1[0];           //PK2
 *        VGS_VAL        =ADC_OUT_1[1];           //PK3
 *
 *This firmware has been implementaed for the IPMS interlock system for BARC project
 *It has adc sampling rate per channel is  200KSPS  and datalogging rate as per Anexure to PO.
 *1000 Data points are stored in flash memory
 *
 *Initially on Power on it will check and wait for the Ethernet connection from server as this device works as a client.
 *It has been assigned with static IP , for dynamic IP do the changes in tcpecho.cfg file
 *
 *command from server============================================
 *For the start of monitoring, control and data transfer use "start"
 *For halting monitoring, control and data transfer use "stopd"
 *For reading data from flash storage use "flash" ,this will work only when device is halted.
 *For erasing flash content use "erase". If flahs was not erased than it will retain last data, hence during next read it may have old data.
 *For system reset like power on reset use "reset". this command will reset the device like power on reset and hence, it will close ethernet connection,----
 * -----and request new connection from server, as connection established, it will wait for start command to run again.
 *
 *
 * Implementation Pending ============================================================
 * start and stop using FROM MAIN signal
 * Staus signal using TO MAIN Signal
 *
 * Indication OF leds - For ethernet , default LEDs used
 *
 *
 */


/*
 *    ======== tcpEcho.c ========
 */

/* XDCtools Header files */
#include <stdint.h>
#include <stdio.h>
#include <stdbool.h>
#include <string.h>
#include <stdlib.h>
#include <math.h>

#include <xdc/std.h>
#include <xdc/cfg/global.h>
#include <ti/sysbios/hal/Hwi.h>

#include <xdc/runtime/Error.h>
#include <xdc/runtime/Memory.h>
#include <xdc/runtime/System.h>

/* BIOS Header files */
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Clock.h>
#include <ti/sysbios/knl/Task.h>

 /* NDK Header files */
#include <ti/ndk/inc/netmain.h>
#include <ti/ndk/inc/_stack.h>

/* TI-RTOS Header files */
#include <ti/drivers/GPIO.h>
#include <ti/sysbios/knl/Semaphore.h>
/* Example/Board Header files */
#include "Board.h"


#include <time.h>

#include "inc/hw_types.h"
#include "inc/hw_memmap.h"
#include "driverlib/sysctl.h"
#include "inc/hw_gpio.h"
#include "driverlib/gpio.h"
#include "inc/hw_ints.h"
#include "driverlib/interrupt.h"
#include "driverlib/timer.h"
#include "driverlib/pin_map.h"
#include "driverlib/adc.h"
//#include "driverlib/rom.h"
//#include "driverlib/rom_map.h"
#include "inc/hw_i2c.h"
#include "driverlib/i2c.h"

#include "driverlib/ssi.h"

#include "inc/hw_flash.h"
#include "driverlib/flash.h"
#include <ti/sysbios/hal/Timer.h>
//#define  dma       false
//#define  flash_en  true


#include <lcd.h>

//============================Ethernet ========================//

#define TCPPACKETSIZE 1024
#define TCPPORT 8080
#define NUMTCPWORKERS 3
#define BUF_SIZE 12412


#define FLASH_BASE_ADDR_RFF         ((uint32_t *)0x00020000)

#define TASKSTACKSIZE   512

Int resource = 0;
Int finishCount = 0;
UInt32 sleepTickCount;

char thbuffer[10];
SOCKET lSocket;
struct sockaddr_in sLocalAddr;

Timer_Params Timer2;
Timer_Handle myTimer;


uint32_t timecounter;
//============================SYSTEM CLOCK========================//
uint32_t g_ui32SysClock;
//============================================================//

int checkLinkState(void)
    {
        return EMAC_isLinkUp(0);
    }


void timerIntHandler(void)
{
    TimerIntClear(TIMER2_BASE, TIMER_TIMA_TIMEOUT);         // must clear timer flag FROM timer
    timecounter++;
}
// Timer start
//void Timer_Start(void)
//{
//    Timer_start(myTimer);
//}
//
//// Timer stop
//void Timer_Stop(void)
//{
//    Timer_stop(myTimer);
//}
//=======================================================================//
// Timer configuration as RTOS base
void timer_init(void)
{
  uint32_t ui32Period;

       //Set CPU Clock to 40MHz. 400MHz PLL/2 = 200 DIV 5 = 40MHz
       SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN);


      // Timer 2 setup code
      SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER2);           // enable Timer 2 periph clks
      TimerConfigure(TIMER2_BASE, TIMER_CFG_PERIODIC);        // cfg Timer 2 mode - periodic

      ui32Period = (SysCtlClockGet() /1000);
      TimerLoadSet(TIMER2_BASE, TIMER_A, ui32Period);         // set Timer 2 period

      IntEnable(INT_TIMER2A);
      TimerIntRegister(TIMER2_BASE, TIMER_A, timerIntHandler);
      IntRegister(INT_TIMER2A, timerIntHandler);

      TimerIntEnable(TIMER2_BASE, TIMER_TIMA_TIMEOUT);        // enables Timer 2 to interrupt CPU
      TimerEnable(TIMER2_BASE, TIMER_A);                      // enable Timer 2
      IntMasterEnable();
}
//void Timer_init()
//{
//      timer_init();
//      Timer_Params_init(&Timer2);
//      Timer2.arg=0;
//      Timer2.period= 500; // 20us
//      //Timer2.period= 1000; //1 ms (Milliseconds)
//      //Timer2.period= 800; //800 us (Microseconds)
//      Timer2.periodType=Timer_PeriodType_MICROSECS;
//      myTimer=Timer_create(2,(Timer_FuncPtr)timerIntHandler,&Timer2,NULL);
//      Timer_start(myTimer);
//
//       //Timer_stop(myTimer);
//
//}


/*
 *  ======== tcpHandler ========
 *  Creates new Task to handle new TCP connections.
 */
Void tcpHandler(UArg arg0, UArg arg1)
{
    fdOpenSession(TaskSelf());

    lSocket = socket(AF_INET, SOCK_STREAM, IPPROTO_TCP);
    if (lSocket < 0)
    {
       // System_printf("tcpHandler: socket failed\n");
        Task_exit();
        return;
    }

    memset((char *)&sLocalAddr, 0, sizeof(sLocalAddr));
    sLocalAddr.sin_family = AF_INET;
    sLocalAddr.sin_addr.s_addr = inet_addr("192.168.1.130");//htonl(INADDR_ANY);
    sLocalAddr.sin_port = htons(arg0);






    while(connect(lSocket, (struct sockaddr *)&sLocalAddr, sizeof(sLocalAddr)) < 0)
    {
        SysCtlDelay(400000);

    }






}


/*
 *  ======== main ========
 */
int main(void)
{
//    Task_Handle taskHandle;
//    Task_Params taskParams;
//    Error_Block eb;

    g_ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |SYSCTL_OSC_MAIN | SYSCTL_USE_PLL |SYSCTL_CFG_VCO_480), 120000000);


    /* Call board init functions */
    Board_initGeneral();
    Board_initGPIO();
    Board_initEMAC();

    /***********************GPIO FOR LEDs*************************/
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOK);
    GPIOPinTypeGPIOOutput(GPIO_PORTK_BASE,GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2);
    GPIODirModeSet(GPIO_PORTK_BASE,GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2,GPIO_DIR_MODE_OUT);
    GPIOPinWrite(GPIO_PORTQ_BASE, GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2, 0x00);

    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
    GPIOPinTypeGPIOOutput(GPIO_PORTE_BASE,GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2);
    GPIODirModeSet(GPIO_PORTE_BASE,GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2,GPIO_DIR_MODE_OUT);
    GPIOPinWrite(GPIO_PORTE_BASE, GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2, 0x00);
    /***********************GPIO FOR SNAP1 & 2*************************/
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
    GPIOPinTypeGPIOOutput(GPIO_PORTL_BASE,GPIO_PIN_4|GPIO_PIN_5);
    GPIODirModeSet(GPIO_PORTL_BASE,GPIO_PIN_4|GPIO_PIN_5,GPIO_DIR_MODE_OUT);
    GPIOPinWrite(GPIO_PORTL_BASE, GPIO_PIN_4|GPIO_PIN_5, 0x00);



    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOM);
    GPIOPinTypeGPIOOutput(GPIO_PORTM_BASE,GPIO_PIN_0);
    GPIODirModeSet(GPIO_PORTM_BASE,GPIO_PIN_0,GPIO_DIR_MODE_OUT);
    GPIOPinWrite(GPIO_PORTM_BASE, GPIO_PIN_0, 0x00);

    timer_init();
    while(1)
    {
        GPIOPinWrite(GPIO_PORTE_BASE, GPIO_PIN_0, 0x00);
        SysCtlDelay(g_ui32SysClock/3);
        GPIOPinWrite(GPIO_PORTE_BASE, GPIO_PIN_1, 0x00);
        SysCtlDelay(g_ui32SysClock/3);
        GPIOPinWrite(GPIO_PORTE_BASE, GPIO_PIN_2, 0x00);
        SysCtlDelay(g_ui32SysClock/3);

        GPIOPinWrite(GPIO_PORTK_BASE, GPIO_PIN_0, 0x00);
        SysCtlDelay(g_ui32SysClock/3);
        GPIOPinWrite(GPIO_PORTK_BASE, GPIO_PIN_1, 0x00);
        SysCtlDelay(g_ui32SysClock/3);
        GPIOPinWrite(GPIO_PORTK_BASE, GPIO_PIN_2, 0x00);
        SysCtlDelay(g_ui32SysClock/3);



        GPIOPinWrite(GPIO_PORTE_BASE, GPIO_PIN_0, GPIO_PIN_0);
        SysCtlDelay(g_ui32SysClock/3);
        GPIOPinWrite(GPIO_PORTE_BASE, GPIO_PIN_1, GPIO_PIN_1);
        SysCtlDelay(g_ui32SysClock/3);
        GPIOPinWrite(GPIO_PORTE_BASE, GPIO_PIN_2, GPIO_PIN_2);
        SysCtlDelay(g_ui32SysClock/3);

        GPIOPinWrite(GPIO_PORTK_BASE, GPIO_PIN_0, GPIO_PIN_0);
        SysCtlDelay(g_ui32SysClock/3);
        GPIOPinWrite(GPIO_PORTK_BASE, GPIO_PIN_1, GPIO_PIN_1);
        SysCtlDelay(g_ui32SysClock/3);
        GPIOPinWrite(GPIO_PORTK_BASE, GPIO_PIN_2, GPIO_PIN_2);
        SysCtlDelay(g_ui32SysClock/3);


        GPIOPinWrite(GPIO_PORTL_BASE, GPIO_PIN_4|GPIO_PIN_5, GPIO_PIN_4|GPIO_PIN_5);
        SysCtlDelay(g_ui32SysClock/3);

        GPIOPinWrite(GPIO_PORTL_BASE, GPIO_PIN_4|GPIO_PIN_5, 0x00);
        SysCtlDelay(g_ui32SysClock/3);

        GPIOPinWrite(GPIO_PORTM_BASE, GPIO_PIN_0, GPIO_PIN_0);
        SysCtlDelay(g_ui32SysClock/3);

        GPIOPinWrite(GPIO_PORTM_BASE, GPIO_PIN_0, 0x00);
        SysCtlDelay(g_ui32SysClock/3);


    }




    /* Start BIOS */
    BIOS_start();

    return (0);
}