after connecting tool ideally green led should turned on ,But not led is turning on or Blinking.
please suggest troubleshooting method.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
after connecting tool ideally green led should turned on ,But not led is turning on or Blinking.
please suggest troubleshooting method.
A couple of suggestions:
1. Present in Device Manger: For the JTAG debug probe to communicate the PC, the driver files need to be installed. This typically occurs co-incident to the installation of the Code Composer Studio (CCS). To verify that the drivers are successfully installed, connect the PC to the JTAG debug probe and power up. Then go to Control Panel → Device Manager (Figure 4-1) and locate the associated debug probe.
2. Reprogram Emulation Controller: This step ensures that the device that functions as the emulation controller has the correct firmware.
XDS110: The host device is a TI MCU TM4C1294NCPDRI3R following guide for re-programming: https://www.ti.com/lit/ug/sprui94/sprui94.pdf
You can find other debug suggestions here: