Part Number: TM4C1292NCPDT
Hello,
We’re connecting TI launchpad to the adapter board having ADUM3151 isolator soldered on it (attached image_01) and giving 3.3V supply and SPI clock signal to the isolator.

While we're able to see the SPI clock signal on Side 1 of the isolator (as shown) but we're not getting any output signals on Side 2.

The current consumed on both the sides of the isolator is: IDD1: 2.8mA (1.5MHz) and IDD2: 5.4mA (1.5 MHz)
On Side 2 of the isolator, we’re giving 8mA as supply current (see image_02) and the current consumed is 5.4mA (image_03) but when we reset the TI eval board, the LED of constant current(CC) starts glowing in the power supply and voltage drops from 3.3V to 2.6V (image_04) and we’re not getting any outputs on the signals of Side 2.
image_02 image_03 image_04