Dear Team,
I am using Quad SPI Master with 60 MHz Bitrate and 10 MHz it working fine and above Frequency SPI CLK Pulse is not proper.
1. what is the SPI Master Quad SPI Maximum frequency With SYSTEM CLK 120Mhz .
2. What configuration required to do continues data transfer in SPI without any delay between SPI CLK Pulse by Setting Chip select low in single transfer.
3. How to use DMA in SPI data send and receive and using DMA will create any delay in SPI Data transfer compared to normal Method.
4. I want to transfer data using SPI without any delay between each byte data transfer .
5. The Switch between SPI Quad mode write and read at run is possible.
Kindly provide Quad Mode Frame format for master and slave mode and Quad Mode Configuration Example code.
Regards,
Naga Narasimha Rao