This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: Questions about PRU-ICSSG for AM2434

Part Number: AM2434


Hello there,

The AM2434 has two PRU-ICSSGs, but which functions can be used at the same time?

For example, can I enable 2 x GMAC, 1 x UART, 1x ECAP, 9 x ΣΔ, 4 x PWM on each PRU-ICSSG and use them simultaneously?

Also, there is an Encoder with 9 x ΣΔ, but how many channels can the Encoder support with one PRU-ICSSG?

Thenk you,

Ryuto

  • Hi Ryuto,

    Apologies for the delay.

    The AM2434 has two PRU-ICSSGs, but which functions can be used at the same time?

    It depends on the pin availability. You can use the syscfg pin mux tool to know the exactly number.

    Also, there is an Encoder with 9 x ΣΔ, but how many channels can the Encoder support with one PRU-ICSSG?

    It can support max up to 9 channels, again the constraint is on pin availability.

    BR

    Nilabh A.