Part Number: TMS570LC4357
using custom board with the TMS5704357 Hercules.
have built 12 boards...all work perfectly.
Using a Blackhawk USB200 jtag emulator
On one of the boards...open code composer, build project, click "debug"...see the chip being erased...see code being loaded...then it doesnt stop at the "main" as usual....
only option is to "terminate.
Appears the jtag is connecting and doing what it is suppose to do...
just looking for possible cause....?....something i can check...
as stated...every other board works.. just this pia one....
see the "nerror" led (ihave connected to herc) go out during the erase and load phase...
if I power board down after doing all the above, it doesnt turn back on and run the code application (even though the CC screen shows it erased and loaded).
tried putting breakpoint in the "main"...that didnt do anythingCC terminates.docx
appreciate any clues/checks.,..
thank you very very much as usual