Part Number: AM2434
The following PAD Configuration Registers are unassigned in "Table 6-1. Pin Attributes (ALV, ALX Packages)" on the datasheet, but each of them is described in the notes for "Table 6-44. GPMC0 Signal Descriptions" or "Table 6-62. MMC1 Signal Descriptions".
PADMMR_PADCONFIG32 000F 4080h
PADMMR_PADCONFIG164 000F 4290h
For GPMC0_CLK:
"The RXACTIVE bit of the CTRLMMR_PADCONFIG32 register must be set to 0x1 and the TX_DIS bit of the CTRLMMR_PADCONFIG32 register must be reset to 0x0 when GPMC0 is operating in synchronous mode."
For MMC1_CLK:
"For MMC1_CLK signal to work properly, the RXACTIVE bit of the CTRLMMR_PADCONFIG164 register must remain in its default state of 0x1 for retiming purposes."
In Table 6-1, PADCONFIG31 is assigned for GPMC0_CLK and PADCONFIG163 for MMC1_CLK.
Must each of PADCONFIG32 and PADCONFIG164 be set as described in the notes for Table 6-44 or Table 6-62?
If not, can each be left at its default (reset value)?
Best regards,
Daisuke