This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432E411Y: Reset Cause from RESC Register Says EXT but RST Pin Doesn't Go Low Enough

Part Number: MSP432E411Y

We are seeing the MSP432E411Y reset with RESC register value 0x00001, indicating the EXT bit in RESC is set.  The TRM (SLAU723A) table 4-17 indicates that this is caused by RST assertion.  However, probing the RST line with a scope probe doesn't seem to show that it should be getting triggered.\

Are there other causes of the EXT bit in RESC getting set than the RST pin going low (< .35*VDD) for 250ns or longer?

Thanks!