This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-AM243: Questions for GTC(Global Timebase Counter)

Part Number: LP-AM243

Hi,

My customer is evaluating LP-AM243 and found below two questions.
Could you answer them?

Q1) How to clear GTC counter value.
According to TRM (SPRUIM2E), Table 12-5294 and Table 12-5297 description.
The counter value can be cleared to zero by writing zero to these register while the counter is disabled (GTC0_GTC_CFG1.EN=0).
The customer tried it, but it does not work. The counter value was unchanged.
Could you tell me how to clear the counter?

Q2) GTC0_GTC_CFG3 physical address
It seems address mismatch in Table 12-5314. GTC0_GTC_CFG3 Registers.
If base address is 00AB 0000h, physical address for GTC0_GTC_CFG3 should be 00AB 0008h.
Which one is correct?




Thanks and regards,
Koichiro Tashiro