Part Number: AM2431
Hello,
We were checking the power rails on our project with the AM243x MCU and found the 1.8V rails are on the edge of failing this power up ramp slew rate below:

What is exactly required by the internal ESD devices here? Does it only requires a slew of >100us from 0V to VDDA(Min) of 1.71V? But the descriptions in 7.10.2.1 made it also sound like the slew rate cannot be bigger than 18mV/us for the entire ramp time – in our case the step part of the ramp at the beginning is failing the requirement.
Thanks,
Fang