Customer designing board. As given in schematic checklist, CAP_VDDSHV_MMC1 need 3.3uF. What is tolerance of capacitance put on CAP_VDDSHV_MMC1?? could it be 4.7uF? Is 2.2uF+1uF ok instead?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Customer designing board. As given in schematic checklist, CAP_VDDSHV_MMC1 need 3.3uF. What is tolerance of capacitance put on CAP_VDDSHV_MMC1?? could it be 4.7uF? Is 2.2uF+1uF ok instead?
Hi Lawrence,
For that particular capacitor, we recommend using a nominal 3.3uF capacitor. That pin is feeding an on-die LDO. The feedback stability analysis on that supply is done based around the 3.3uF nominal value. Also, if starting with too small of a cap, over time with aging, that might degrade the performance of the LDO. Please use the recommended 3.3uF.
This is in contrast to the normal decoupling on the core, IO and clock power nets where substitutions can be made from our initial recommendations as long as the overall resulting PDN transient response is still sufficient.
Thank you,
-Randy
Hi Randy,
is it ok to use 2.2uF +1uF? Issue is 3.3uF are difficult to source
Regards,
Lawrence
Hi Lawrence,
I think that would be fine. Just make sure to mount them right next to each other in the layout.
Thank you,
-Randy