This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129ENCPDT: Wolfssl Cert Validation with TM4C TIRTOS

Part Number: TM4C129ENCPDT


Hello,

I am using the TM4C129ENCPDT and I made a mistake in the PCB layout where I forgot to add the external 32KHz crystal connected to the XOSC pins. I am using TI-RTOS and wolfssl in this project to connect to a TLS server. I also have an external RTC chip with an internal crystal in the design that I use to keep time and for other alarm purposes. I am able to successfully connect to an NTP server, obtain time and then update my RTC. After some calculations, the time I get from NTP is what I pass on to the "Seconds" function, which I believd will be used to validate the time in my TLS certificate.

Here's the problem I am having: Since I forgot to add the external 32KHz crystal. my program gets stuck in the "Seconds" function. It looks like this has something to do with the hibernation module but I am not entirely sure. At least for now, for the 5 prototype boards I built for testing, what I did was comment out "Seconds" function and bypass cert validation by using "WOLFSSL_VERIFY_NONE" so I could connect to my TLS server and not delay our development.

My question is, is there a way to implement cert validation without having to install that 32KHz crystal? Is there some alternate settings that would let me use "Seconds" function and WOLFSSL_VERIFY_PEER. I was wondering if there is an internal 32KHz I could use. The reason I decided not to place the 32KHz crystal to the XOSC is because I am not using the built in RTC or the Hibernation module for anything. I didn't know the "Seconds" function would get stuck without it. And I am already using an external RTC for my timekeeping. If I can make this work without the 32KHz crystal, it would really save us time and money and I wouldn't have to scrap some boards and redo layout.

Thanks in advance. Any input is much appreciated.

Regards,

AJ 

 

 

  • Hi AJ,

    My question is, is there a way to implement cert validation without having to install that 32KHz crystal? Is there some alternate settings that would let me use "Seconds" function and WOLFSSL_VERIFY_PEER. I was wondering if there is an internal 32KHz I could use. The reason I decided not to place the 32KHz crystal to the XOSC is because I am not using the built in RTC or the Hibernation module for anything. I didn't know the "Seconds" function would get stuck without it. And I am already using an external RTC for my timekeeping. If I can make this work without the 32KHz crystal, it would really save us time and money and I wouldn't have to scrap some boards and redo layout.

    Sorry, I wish I could help you here. However, I don't have knowledge about TLS and WolfSSL stacks. I don't know the purpose why TLS would require a 32kHz OSC. I suggest you contact WolfSSL experts it the TLS protocol would require the presence of 32Khz in the design. This way you can rule out if the problem is software related or really requiring a 32kHz OSC. 

      I found this example sntp code which is simpler than ntp protocol. Not sure if this will help you. 

    /*
     * Copyright (c) 2015-2021, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     */
    
    /*
     *  ======== sntp.c ========
     *  SNTP Client example application
     */
    #include <string.h>
    #include <time.h>
    
    /* XDCtools Header files */
    #include <xdc/runtime/Error.h>
    #include <xdc/runtime/System.h>
    
    /* TI-RTOS Header files */
    #include <ti/sysbios/BIOS.h>
    #include <ti/sysbios/hal/Seconds.h>
    #include <ti/sysbios/knl/Task.h>
    #include <ti/sysbios/knl/Semaphore.h>
    #include <ti/drivers/GPIO.h>
    #include <ti/net/http/httpcli.h>
    #include <ti/net/sntp/sntp.h>
    
    /* Example/Board Header file */
    #include "Board.h"
    
    #include <sys/socket.h>
    
    /*
     * NTP server and port to obtain network time and number of servers to attempt
     */
    #define NTP_HOSTNAME "north-america.pool.ntp.org"
    #define NTP_PORT         "123"
    #define NTP_SERVERS      3
    #define NTP_SERVERS_SIZE (NTP_SERVERS * sizeof(struct sockaddr_in))
    #define NTPTASKSTACKSIZE 2048
    
    /*
     * Time Zone Adjustment.
     * TODO: Adjust your local time zone with respect to Greenwich Mean Time (GMT)
     * For example, North America Central Time Zone is 6 hours behind GMT
     */
    #define CENTRAL_TIME_ADJUST -6*60*60
    #define TIME_ZONE_ADJUST CENTRAL_TIME_ADJUST
    
    unsigned char ntpServers[NTP_SERVERS_SIZE];
    static Semaphore_Handle semHandle = NULL;
    
    /*
     *  ======== printError ========
     */
    void printError(char *errString, int code)
    {
        System_printf("Error! code = %d, desc = %s\n", code, errString);
        BIOS_exit(code);
    }
    
    /*
     *  ======== timeUpdateHook ========
     *  Called after NTP time sync
     */
    void timeUpdateHook(void *p)
    {
        Semaphore_post(semHandle);
    }
    
    /*
     *  ======== startNTP ========
     *  This is the function that generates the request to the NTP server for network time.
     */
    void startNTP(void)
    {
        int ret;
        int currPos;
        time_t ts;
        struct sockaddr_in ntpAddr;
        struct addrinfo hints;
        struct addrinfo *addrs;
        struct addrinfo *currAddr;
        Semaphore_Params semParams;
    
        /*
         * Clear the addrinfo first.
         */
        memset(&hints, 0, sizeof(struct addrinfo));
    
        /*
         * Use SOCK_DGRAM (UDP) as the socket type
         */
        hints.ai_family = AF_INET;
        hints.ai_socktype = SOCK_DGRAM;
    
        /*
         * First resolve the IP Address of the NTP server using the DNS service..
         * The getaddrinfo can return a linked-list of IP addresses
         */
        ret = getaddrinfo(NTP_HOSTNAME, NTP_PORT, NULL, &addrs);
        if (ret != 0) {
            printError("startNTP: NTP host cannot be resolved!", ret);
        }
    
        currPos = 0;
    
        /*
         * Loop through the NTP servers
         */
        for (currAddr = addrs; currAddr != NULL; currAddr = currAddr->ai_next) {
            if (currPos < NTP_SERVERS_SIZE) {
                ntpAddr = *(struct sockaddr_in *)(currAddr->ai_addr);
                /*
                 * Copy the list of NTP servers to netServers
                 */
                memcpy(ntpServers + currPos, &ntpAddr, sizeof(struct sockaddr_in));
                currPos += sizeof(struct sockaddr_in);
            }
            else {
                break;
            }
        }
    
        freeaddrinfo(addrs);
    
        /*
         * Initialize and start the SNTP client Task. Called to create and start SNTP
         * client Task and Semaphores. User must pass in pointers to functions for
         * getting and setting the current time and the list of NTP servers to
         * communicate with. timeUpdateHook() is called upon successful time
         * synchronization.
         */
        ret = SNTP_start(Seconds_get, Seconds_set, timeUpdateHook,
                (struct sockaddr *)&ntpServers, NTP_SERVERS, 0);
        if (ret == 0) {
            printError("startNTP: SNTP cannot be started!", -1);
        }
    
        /*
         * Create a semaphore that will block until after successful NTP time
         * synchronization.  Once unblocked, we will print the current time to the
         * console.
         */
        Semaphore_Params_init(&semParams);
        semParams.mode = Semaphore_Mode_BINARY;
        semHandle = Semaphore_create(0, &semParams, NULL);
        if (semHandle == NULL) {
            printError("startNTP: Cannot create semaphore!", -1);
        }
    
        SNTP_forceTimeSync();
        /*
         * Wait here until the semaphore is posted.
         */
        Semaphore_pend(semHandle, BIOS_WAIT_FOREVER);
    
        /*
         * Adjust for the Central Time Zone.
         */
        Seconds_set((unsigned int)((int)Seconds_get()+TIME_ZONE_ADJUST));
        ts = time(NULL);
    
        /*
         * Print the current time to the console.
         */
        System_printf("Current time: %s\n", ctime(&ts));
        System_flush();
    
    }
    
    /*
     *  ======== netIPAddrHook ========
     *  This function is called when IP Addr is added/deleted
     */
    void netIPAddrHook(unsigned int IPAddr, unsigned int IfIdx, unsigned int fAdd)
    {
        static Task_Handle taskHandle;
        Task_Params taskParams;
        Error_Block eb;
    
        /* Create a NTP task when the IP address is added */
        if (fAdd && !taskHandle) {
            Error_init(&eb);
    
            Task_Params_init(&taskParams);
            taskParams.stackSize = NTPTASKSTACKSIZE;
            taskParams.priority = 1;
            taskHandle = Task_create((Task_FuncPtr)startNTP, &taskParams, &eb);
            if (taskHandle == NULL) {
                printError("netIPAddrHook: Failed to create NTP Task\n", -1);
            }
        }
    }
    
    /*
     *  ======== main ========
     */
    int main(void)
    {
        /* Call board init functions */
        Board_initGeneral();
        Board_initGPIO();
        Board_initEMAC();
    
        /* Turn on user LED */
        GPIO_write(Board_LED0, Board_LED_ON);
    
        System_printf("Starting the SNTP example\nSystem provider is set to "
                "SysMin. Halt the target to view any SysMin contents in ROV.\n");
        /* SysMin will only print to the console when you call flush or exit */
        System_flush();
    
        /* Start BIOS */
        BIOS_start();
    
        return (0);
    }
    
    sntp.cfg

  • Charles, thank you for your response. I think I figured out how to fix the problem. What I did was use the internal 32KHz by calling the function HibernateClockConfig(HIBERNATE_OSC_LFIOSC) before calling Seconds_Set(). This solved the problem.

    Regards,

    AJ