Part Number: TMS570LC4357
Hi,
I would like to confirm what is the maximum current going through the PLL supply voltage pin which is a single terminal (terminal no. : P11) in the TMS570LC4357
Thanks
Roberto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LC4357
Hi,
I would like to confirm what is the maximum current going through the PLL supply voltage pin which is a single terminal (terminal no. : P11) in the TMS570LC4357
Thanks
Roberto
Hi Roberto,
We don't have value of current consumed by VCC PLL only.
--
Thanks & regards,
Jagadish.
Hi- thanks for the support. So how should I approach to size (in terms of current rating) any circuitry connected to that supply input? such us a Low pass filter.
As the combined spec is 990mA spread across VCCPLL + VCC (12 BGAs terminals in total), as an asssumption would it be acceptable to divide the current seen by the pin as 990mA / 12
Thanks
Hi Roberto,
As the combined spec is 990mA spread across VCCPLL + VCC (12 BGAs terminals in total), as an asssumption would it be acceptable to divide the current seen by the pin as 990mA / 12
It is not ideal way to do it, the current on VCCPLL will depends on PLL related configurations inside the controller. So, i will discuss with my internal team and get back to you on this.
--
Thanks & regards,
Jagadish.
Hi Roberto,
Theoretically the PLL current is typically under 10mA, but because there are two PLLs, the pin could see 20mA.
When we did practical measurement for one of our Hercules boards we got, current at idle (CPU suspends at a breakpoint in main()) is around 2.3mA (PLL1=PLL2=180MHz), and the current when performing SRAM reading and writing is around 3.2mA. Same measurement will be applicable for LC4357 as well.
--
Thanks & regards,
Jagadish.