Part Number: TMS570LS1224
Other Parts Discussed in Thread: HALCOGEN
Hello everyone,
I am currently attempting to configure communication with an SD card over SPI on my Hercules processor and I came across the following blog post:
I coulnd't download the link from the blog post, but I downloaded the library from another topic, the version is: "6428.RM48 HDK RevE SDCard Demo.zip"
I attached my project folder.
I build the file with only warnings, but could not figure out why it wount work...
My Board conection is:
SD Adapter -----> TMS570LS1224
CS ----------------> 3CS1 (J5 pin 18)
SDK --------------> 3CLK (J2 pin 7)
MOSI ------------> 3SOMI (J5 pin 14)
MISO ------------> 3SIMO (J5 pin 15)
VCC -------------> 3.3V (J2 pin 1)
GND ------------> GND (J3 pin 22)
Could someone help to make this work?
Thank you