Part Number: AM2432
The Setup & Problem
- We are on CCS 12.1
- We have an automated test setup with one Linux headless machine connect to multiple/four XDS110
- Each XDS110 is connect to one PCB with a AM2432 part.
- We are trying to load a .out file/image to each of the PCB using Loadti or DSS script.
- How can we specify a particular XDS110 device in LoadTi or DSS script ?
Serial Number for all 4 XDS110 are the same
Using xdsdfu to display the XDS device connect, it is show that the serial numbers are the same:
$ /home/AndyToronto/ti/ccs1210/ccs/ccs_base/common/uscif/xds110/xdsdfu -e
USB Device Firmware Upgrade Utility
Copyright (c) 2008-2019 Texas Instruments Incorporated. All rights reserved.
Scanning USB buses for supported XDS110 devices...
<<<< Device 0 >>>>
VID: 0x0451 PID: 0xbef3
Device Name: XDS110 Probe with CMSIS-DAP
Version: 2.3.0.5
Manufacturer: Texas Instruments
Serial Num: 00000000
Mode: Runtime
Configuration: Standard
<<<< Device 1 >>>>
VID: 0x0451 PID: 0xbef3
Device Name: XDS110 Probe with CMSIS-DAP
Version: 3.0.0.22
Manufacturer: Texas Instruments
Serial Num: 1234
Mode: Runtime
Configuration: Standard
<<<< Device 2 >>>>
VID: 0x0451 PID: 0xbef3
Device Name: XDS110 Probe with CMSIS-DAP
Version: 2.3.0.5
Manufacturer: Texas Instruments
Serial Num: 00000000
Mode: Runtime
Configuration: Standard
<<<< Device 3 >>>>
VID: 0x0451 PID: 0xbef3
Device Name: XDS110 Probe with CMSIS-DAP
Version: 3.0.0.22
Manufacturer: Texas Instruments
Serial Num: 00000000
Mode: Runtime
Configuration: Standard
Found 4 devices.