Part Number: LP-AM243
Hello,
I am trying to read multiple 16bit words over SPI from an external ADC.
I can see the frames I need on a logic analyzer but when I read the MCSPI_RX register I keep getting just the first word multiple times instead of the remaining elements in the RX FIFO.

This is my code:
/* SPIEN line is forced to low state.*/
MCSPI_writeChConfReg(baseAddr, chNum, gCsAssertRegVal);
while(transferLength!=0)
{
/* Write Effective RX FIFO depth */
if (transferLength >= effRxFifoDepth)
{
transferLength = effRxFifoDepth;
}
while (0 == (MCSPI_readChStatusReg(baseAddr, chNum) &
CSL_MCSPI_CH0STAT_TXFFE_MASK))
{
/* Wait for Tx FIFO to be empty before writing the data. */
}
/*Loops for retrieving the multiple SPI words*/
for(uint8_t i=0;i<transferLength;i++) //transferLength for this example is 2 (bytes)
{
MCSPI_writeTxDataReg(baseAddr, 0x00000000, chNum); //writing dummy TX data
}
for(uint8_t i=0;i<transferLength;i++)
{
rxBuff[i]=(uint16_t)MCSPI_readRxDataReg(baseAddr, chNum); //rxBuff points to Rxbuffer_16
if(en_Chn_Seq_Idx[i]!=0xAA) //writing relevant data into shared memory
{
shmem.ADC_Buff[en_Chn_Seq_Idx[i]][db_idx][curr_dbuf_dpt]=rxBuff[i]; //write data into shm.mem double buffer
}
}
numWordsRead += transferLength;
transferLength = length - numWordsRead;
}
while (0 == (MCSPI_readChStatusReg(baseAddr, chNum) &
CSL_MCSPI_CH0STAT_TXFFE_MASK))
{
//Wait for Tx FIFO to be empty for the last set of data.
}
while (0 == (MCSPI_readChStatusReg(baseAddr, chNum) &
CSL_MCSPI_CH0STAT_EOT_MASK))
{
/* wait for the end of transfer of last word.*/
}
/* Force SPIEN line to the inactive state.*/
MCSPI_writeChConfReg(baseAddr, chNum, gCsDeAssertRegVal);
I used the mcspi performance 32bit example code as a reference for my code.
And the configuration I am using is :
I also noticed that when I go through the code line by line in debug mode, I see the MCSPI_RX register getting updated as it should after each MCSPI_readRxDataReg() function call.
So, I assumed I might not be giving enough time for the MCSPI_RX buffer to be updated with the next element from the FIFO after reading it.
So I tried the below code:
for(uint8_t i=0;i<transferLength;i++)
{
MCSPI_writeTxDataReg(baseAddr, 0x00000000, chNum);
while(0 == (MCSPI_readChStatusReg(baseAddr, chNum) &
CSL_MCSPI_CH1STAT_RXS_FULL))
{
/*wait till element is read into the fifo*/
}
rxBuff[i]=(uint16_t)MCSPI_readRxDataReg(baseAddr, chNum);
if(en_Chn_Seq_Idx[i]!=0xAA) //writing relevant data into shared memory
{
shmem.ADC_Buff[en_Chn_Seq_Idx[i]][db_idx][curr_dbuf_dpt]=rxBuff[i]; //write data into shm.mem double buffer
}
}
The difference being, Instead of reading the MCSPI_RX register in a loop, I wait for RXS bit of the MCSPI Status register to be FULL before reading the MCSPI_RX register for the next word.
This seems to work, but it introduces additional delay between two words which is undesirable.
Is there anyway to read MCSPI_RX register without having to wait for any status bits?
Am I approaching this issue the right way?
Thanks and Regards.