Part Number: TM4C1292NCPDT
Hi,
In reference to the following post;
Please guide on how is the series resistor value decided for the connection.
In my circuit, I'm connecting the output of optocoupler to a GPIO pin of microcontroller configured as input (signal 'DIN_SRC_SINKSEL1'). On the input side, I'm giving a signal of 24V and output is 3.3V.

I want to calculate the series resistor value in the path from the output of optocoupler to the microcontroller (assuming 2mA current being supplied to the microcontroller).
When I'm checking the current across the series resistor 10E or 1K, it's not showing any current drop.
Thanks,
Kiran